AnsweredAssumed Answered

LabVIEW programming 34905A RF MUX card

Question asked by AlphaBob on Dec 12, 2017

Question about the 14905A RF MUX. Looking at the example LabVIEW code it says:

 

The HP34907A has two banks which have 4 channels each.  Only one chanel may be closed on each bank.

 

(Yes it still says "HP")

 

But anyway I can see this uses the same LabVIEW vi as the 34903A 20 Channel Actuator/GP Switch Module. That make sense as the RF MUX is just relays.

 

My question is it says only one channel may be closed on each bank. Does that mean I do not have to open previous channel before closing the next?

 



Outcomes