I was wondering if anyone has run into this issue. I have been using the commands "CALCulate<cnum>:DATA:SNP:PORTs? for reading SNP and
"CALCulate<cnum>:DATA:SNP:PORTs:SAVE <"x,y,z">,<filename>" to remotely save s2p data to a specified file path.
On the first command, the Command Expert is prompting for x,y,z input but there is no field available to enter.
On the second command for saving SNP, Command Expert (v1.7) throws up error as: SCPI Error, 103 CALC measurement selection to none.
Listed below is the model and firmware information for the affected analyzer. Thanks for your time!
PNA-L N5235A
A.9.90.19
This is the command I use for saving SNP data and as a result an error message is thrown up
:CALCulate:DATA:SNP:PORTs:SAVE "1,2","test.s2p"