Hello,
I am using ADS 2015.01. I have created a basic high-speed channel using differential TX/RX. I have realized the channel using "Line Type Component LTLINE2" (Couples Transmission Line). I have also used "Controlled Impedance Line Designer" for desired impedance settings. Now I want to extract the s-parameter file (Touchstone/SnP) from LTLINE2. Can anyone help me how to get that? I will use that s-parameter file for other transceiver in Cadence or ADS. It will be really helpful.
Best regards,
Piash
Run an S-parameter simulation of the coupled line. The resulting dataset can be converted to a Touchstone file using the Data File Tool.