How to use the Verification Test Bench (VTB) provided in ADS to test microstrip patch antenna designed for LTE?
You probably don't need to use a VTB for a linear simulation of a device like an antenna. Suggest using ADS Momentum; there are helpful examples Single_patch and Double_patch in the \Momentum\Antenna folder.
Hello
I do not want to use VTB for simulation of antenna. Rather I want to test the patch antenna designed for LTE by using the LTE VTB provided in ADS.
Please tell me how can I do this?
You probably don't need to use a VTB for a linear simulation of a device like an antenna. Suggest using ADS Momentum; there are helpful examples Single_patch and Double_patch in the \Momentum\Antenna folder.