AnsweredAssumed Answered

Wrong ouput power on Port1 and 2 (E5071B)

Question asked by Andreas on Jul 25, 2007
Latest reply on Jul 31, 2007 by Andreas
Hello,

I´ve got a problem with our E5071B:
The output power on Port 1 and 2 is wrong. I measured it with a Sectrum Analyzer and a 20dB attenuator in order to be sure of the 50 ohms. The output power is 13dB less than the configurated power level in the sweep setup.
I think the measurement of the S-parameters is still ok.

Is there a possibility to calibrate the source power?

Thanks for your answers

Andreas  

Outcomes