我使用100欧姆的电阻测试线路上的静态电流,想知道在用安捷伦电源供电时直接接了补偿的S+ S-,这样会不会影响静态电流的测量
(I used a 100 ohm resistor to test the quiescent current on the line, wondering if the compensated S + S- was connected directly with Agilent's power supply, which would not affect the quiescent current measurement)
Hi,
I'm not sure I understood the question, but the S + and S- terminals are not disconnected internally when the power is turned OFF. You will measure a residual voltage near 0V (some mV), so a very low current in the resistance of 100 Ohms.
我不確定我是否理解這個問題,但是當電源關閉時,S +和S-端子不會在內部斷開。 您將測量接近0V(幾mV)的殘餘電壓,因此100歐姆電阻中的電流非常低。
Yves