AnsweredAssumed Answered

4395A low freq. Z Measurement

Question asked by justoncamm on Jan 4, 2010
Latest reply on Jan 5, 2010 by RayH
I want to measure impedance down to 9kHz. I have a bridge that works to 100kHz, so not wanting to have to purchase an 87512A. Can I use an older 35676B which would appear to do the same job, but to max 200MHz and 75ohm?  

Outcomes