I am doing a transient sim which is supposed to run upto 300ns. I have a 100ns PWL current source that is defined in a table format. I am able to take this current source and convert it into a datasource (.ds) file. I then define an ItDataset component that with Tmax = 300ns. According to the docs, the current is supposed to repeat if Tmax is greater than the current source. However, that is not happening. See attached file showing the currents
Any clues on how to do this