I have a 1680AD logic analyzer with a corrupted hard drive which will no longer boot. It is the version with a Radisys SC815E 1GHz PIII motherboard so I am looking for an .ISO image of the 01680-14100 recovery CD/DVD.
Previously this was available at this location which is now empty:
ftp://ftp.keysight.com/cos/outbound/16xxx%20recovery%20images/01680-14100/
Can the 01680-14100 recovery CD/DVD image be made available again there so I can download it and use it to restore my 1680AD to working condition again?
Also, is an .ISO image of the 16900-14122 BIOS update CD available? The page referenced below says it previously was available here which is now empty:
ftp://ftp.keysight.com/cos/outbound/BIOS/
For reference see: How can I update the BIOS on my Keysight Logic Analyzer?
http://www.keysight.com/main/editorial.jspx?cc=US&lc=eng&ckey=1693762
Hello,
The IT department at Keysight no longer allows data to be left on the ftp site more than 7 days, so everything that was always there was removed, leaving bare directories behind. At about the same time this decision was implemented, the person who kept track of the data you are looking for had a heart attack, and subsequently retired. All notices of this change were sent to his email, which he wasn't watching. As a result, not all data was recovered. Add in the fact that I'm the new guy (only 36 years with the company), taking over this data, and you'll find that not everything is available. I, luckily, had my own private stash of CD's and images that I'm using to fill in where possible
Now to your requests:
- 16800-14100 - That was some of the data that was lost. The -14100 discs were replaced by the -14101 discs, which are supposed to be compatible upgrades. I have put those at: ftp://ftp.keysight.com/cos/outbound/16xxx%20recovery%20images/01680-14101/
Give them a try...
- 16900-14122 - I have put that at: ftp://ftp.keysight.com/cos/outbound/16xxx%20recovery%20images/16900-14122/
Let me know how this works out for you...
Al