AnsweredAssumed Answered

how to solve query interrupted error

Question asked by jungle on Oct 7, 2017
Latest reply on Oct 15, 2017 by jungle

I've seen the same question from BBS, but it can't solve my problem。

I'm going to connect the oscilloscope to the wlan.

It was supposed to be a continuous reading of the data, and later found that it didn't work (and maybe I ignored something).

Then change to extend the oscilloscope to read the waveform time, which is achieved by obtaining more sampling data points.

Then there's the problem.

In ASCii format, everything is fine, but the speed of transmission is too slow.

When using WORD format, when the sample data point is set to exceed 450,000 or less than 40,000, the returned data is completely wrong,And there are query interrupted red tips on the screen。

Hope to solve the problem, thanks.

Attachments

Outcomes