AnsweredAssumed Answered

E5071C Peak tracking

Question asked by reg.mpi on Sep 28, 2017
Latest reply on Sep 29, 2017 by KSuiker

The E5061A has a way to track the peak of an amplified signal and obtain the rejection of the signal, i.e. 40dB points referenced to the peak.  This is accessed via the button sequence:  SCALE--REFERENCE TRACKING--TRACK PEAK.  Is this possible on the E5071C?  I can't find the right sequence of buttons if there is a way, and found nothing in the manual.

 

reg.mpi

Outcomes