Hello,
I want to apply a differential signal input to my rectifier circuit. As i know most of the available measurement equipment are single-ended configuration. If I'm going to use to signal generator for differential feeding, and connecting the GND as common between them. Then the problem how to adjust the signal phase of the 2nd generator to be 180 Degree?
Anyone has any suggestion for the validation of such measurement setup, if it is correct how can I generate phase difference 180?.
The available signal generator is Agilent Agilent E4482C.
Hello mansour001,
It sounds this can be easily done by using a balun or RF transformer without having to use a separate signal generator.
Let us know if this works for you.
Best regards,
Miguel