I am trying to set my AFG 335x channel output impedance to HiZ. I am using IVI 2.3.1.0 x64 driver downloaded from Keysight. Per my understanding of IVI Fgen commands a value of 0 should do this but I see the output set to 1 Ohm instead. I also tried setting it to something very high like 50000 but it gets limited to 10000.
How can I set a value of HiZ?
Hi,
The SCPI Command to place it the generator in HiZ is "OUTP:LOAD INF".
From the IVI Driver Help File:
Best regards,
David