Description:
Step1: Open the example "baseband verification/GNSS/GPS/GPS_CNR_estimation/design1"; change only 1 parameter "BlockNumStop" in G1 from 3 to 9; then everything normal showing G1.CN0R around 42dB;
Step 2: Sweep parameter "NoiseFigure" in A2 from 5 to 6 with step 1; G1.CN0R show normal results around 39dB for all blocks at NF=5dB, but at NF=6dB, some blocks show G1.CN0R abrupt change to -10000
My questions:
1) Is it reasonable for the abrupt change in CN0R when NF only change 1dB; (simulator bug or wrong setting?)
2) What should I do if I want G1.CN0R to show normal value (say around 38dB) instead of -10000?