AnsweredAssumed Answered

De-embedding process with PNA N5227A

Question asked by srlab on Sep 7, 2017
Latest reply on Sep 7, 2017 by daras

Hi all,

I am trying to de-embed a differential input single output amplifier using a PNA N5227A I have been given a guide but when I get to the Measure screen I get a pair of warnings the first is 'Method delete fail, measurement not found' then another following it 'Index was outside the bounds of the array'. If I ignore these I eventually get to saving the file then choosing a screen that indicates 2 ports in the top box then the instructions tell me to select 'multiport' but this box does not appear (in the help file associated with de-embedding at this point it does show the same screen but with the options) I have the general advice file and my tracking file which are both public domain if anyone can isolate where I have gone wrong. Thanks, Phil Swire

Outcomes