How to force the AWG (eg 33500B series) to hold exactly the same last voltage of an arbitrary waveform after having played this ARB waveform? So far, the difference between the last point of an ARB and the DC level hold afterwards can be as large as several tens of mV.
Hi, when you start your sequence, you start with the first point of the sequence and after the end of sequence, generator come back to the first point and wait for next trigger. If you want that generator have same DC level that the last point, the first point must be the same value that the last point.