AnsweredAssumed Answered

34970A on 82357B USB/GPIB assert ren problem

Question asked by solid on Aug 30, 2017
Latest reply on Oct 9, 2017 by solid

Hi,

I'm running a system with an 34970A datalogger on a 82357B USB/GPIB interface. I have several machines connected to the gpib bus and some require NI MAX to operate so i'm running NI VISA as primary with Keysight VISA secondary. I need to enable NI-488 for some of the machine to work but when I do the 34970A stops working ("cannot execute in local mode"). I've tried setting "Assert ren when system controller" in the 82357B config but it will not stay set, always returns to false.

Any ideas?

 

Thanks,

Outcomes