AnsweredAssumed Answered

Fieldfox vna calibration timeout

Question asked by jsmith on Aug 29, 2017
Latest reply on Aug 29, 2017 by tsilchia

Hi I am using VISA IO libraries in a C# .NET application to control a handheld Vector analyzer. The code I am using is here:

 

if(MessageBox.Show("Connect THRU to port 1 and port 2.") == DialogResult.OK)
{

fio.WriteString("CORR:COLL:THRU 1,2", true);
fio.WriteString("*OPC?");
int temp = fio.ReadNumber();
fio.WriteString("CORR:COLL:SAVE 0", true);

}

 

I have set the timeout to 60s but still it gives a timeout error. What am I doing wrong?

Outcomes