RF input is attenuating with machine set to preset, ampd cal reads -20dB on power meter like it should but -48dB on spec an, possible bad attenuator? if i touch the connector quickly to the attenuator the signal is normal but when i fully plug the connector from the rf board into the attenuator the signal attenuates 40dB