AnsweredAssumed Answered

Number of Data Points using 82357B USB-GPIB Interface for 4395A Network/Spectrum/Impedance Analyzer

Question asked by Kolkoori on Aug 22, 2017
Latest reply on Aug 22, 2017 by emcpete

Dear Madam/Sir,

 

I am using the 82357B USB-GPIB interface for acquiring the impedance and phase data from 4395A impedance analyzer. I could not able to get full set of data points and frequency resolution that are available on the impedance analyzer display screen. I am getting only 201 data points for the frequency sweep between 10kHz and 20MHz instead of 4000 data points, which are available on the analyzer display screen.

Could you please help me how to acquire full set of data points using VISA.com software?

 

Looking forward to your kind support.

 

with best regards,

Sanjeev

Outcomes