AnsweredAssumed Answered

How to use U1084A in digitizer mode to collect many segments of data for one reading?

Question asked by HARI on Aug 21, 2017
Latest reply on Aug 23, 2017 by algoss

Dear all,

I would like to ask you,  is it possible that  U1084A   (digitizer -  averager)  to work as  a digitizer not as an averager such that I can store 100 segments with 1000  samples in each segment in a one sequence acquisition ?  In the user manual of U1084A, it says it has 16KS acquisition memory and also it says digitizer mode is only possible for the single segment( only one trigger )?

 

 In the user manual of U1084A, it says it has 16KS acquisition memory and also it says digitizer mode is only possible for the single segment( only one trigger ).

 

 I need to store data per triggers as a sequence of segments in digitizer mode and not in average mode.  

 

Please, could anybody have a solution to my question?

 

 

Thank you for your answers in advance. 

 

Hari

Outcomes