AnsweredAssumed Answered

Agilent 66319D - Minimum and Maximum Currents in DLOG Mode

Question asked by sushant.shidore on Aug 21, 2017

I'm trying to measure average and peak currents of a Bluetooth device.

I can get the average value of the current fine, but to find the peak value, I don't know whether the 'Maximum' current which is shown at the bottom of the Device Characterization software represents the same.

 

What is the significance of and where are the minimum and maximum values coming from?

Sometimes the minimum value is shown negative.

When I select 'Max' and 'Min' in the 'Current Graph Type' option in the left panel, different peaks are shown which are different than those for the DC current measurement.

Outcomes