Dear all,
when I start to capture a curve with the oscilloscope I get the following error message:
Error clearing the scope and setting the trigger. The waveform capture will be disabled.
I don´t know where to set the correct setting. Maybe in "Setup Trigger" (see attached file)?
Thanks in advance
Best regards,
Huelya
You may have a HW problem with your scope. Does AutoScale work?
Try the following:
- Do a Default Setup
- Connect Channel 1 to Aux Out or Cal Out (I've forgotten what this scope has on the front panel) with a cable
- Try AutoScale
Is there a square wave on the screen?