I am working in transmitting side and want to extract the channel parameters in V-series oscilloscope. The AWG M8190 equipped with M9536A embedded controller is connected with PSG vector signal generator, E8267D and the vector signal generator is connected to the DSAV084A, Infinium V-series. But when I worked in the M8190A software named Front panel soft and changed the standard waveform, it did not show any change in the PSG vector signal generator and also in the oscilloscope. What is the problem? I need to generate a wideband signal with carrier frequency 6GHz.
Moved your thread to the Scopes forum for traction.
Thanks,
Jill