Hello,
is it possible to set a low pass filter on a channel of a MSOX3000 or MSOX4000 oscillosopes?
Maybe this is kind of contrary to the oscilloscope philosophy of show signals as they are, but I would be nice to blend out a pwm signal and have a look at what the coil is seeing. I have looked into the averaging the Signal, which is basically a low pass filter, but am not sure how to set it up to have a desired corner frequency needed. Any ideas?
Regards,
John
Yeah, low pass filter is available as a Math function.
See page 118 of the user guide: http://literature.cdn.keysight.com/litweb/pdf/54709-97061.pdf?id=2265134