Hellow all:
I am a complete beginner to useing ADS. After finished the schematic diagram, I begin to simulate the circuit, and the transient simulation is through. But DC simulation has been a failure, when the system gives the following tips:
No DC annotation information is available for this design.
1. If this design is a top-level design that can be simulated, run the simulation to produce the DC annotation information.
If you've run a simulation and there is still no DC annotation information available, it is most likely because the DC solution is not available when running an S-Parameter or AC simulation on a purely linear circuit.
2. If this design is not a simulatable design, go to the top-level, simulatable design and push down into this design using the 'View : Push into Hierarchy' command or the 'Push into Hierarchy' button on the toolbar.
Most of the system configuration is the default, how can I DC simulation?
Thanks for the help!
Please contact your local Technical Support department for assistance. The solution is likely simple, but it's difficult to understand the setup from the post.