I'm using the totalize function of the 53220, which is connected to a 1V, 1 kHz square wave generator. Setting the 53220A in the continuous mode, after triggering I see the number running on the display, where each count corresponds to 1 ms.
Now I need to manually stop the counter. This action has to be manual, because it corresponds to some external event in the lab that can not be converted in a signal. How can be done?