AnsweredAssumed Answered

SCPI command for unratioed(Absolute Power) Measurements

Question asked by Egide on Jun 29, 2017
Latest reply on Jun 29, 2017 by Egide

Hello,

I need the SCPI command sequence to measure absolute power with PNA N5225A while using external power source (1) and while using internal power source (2).


1. Numerator A, Denominator 1.0, Source Port = None. What are the SCPI commands to setup a measurement trace?

2. Numerator A, Denominator 1.0, Source Port = Port 2. What are the SCPI commands to setup a measurement trace?

Outcomes