AnsweredAssumed Answered

Newbie with a dumb question

Question asked by red87droptop on Mar 15, 2008
Latest reply on Mar 18, 2008 by odanzy
Hi, I have an Agilent E4418B power meter with a 8481B sensor with an Agilent 30db attenuator on the end. My question is do I Zero this meter with the attenuator on the end of the sensor connected to the 50mhz power reference or disconnected. I have read in the manual it has to be calibrated without the attenuator and connected to the 50mhz reference but it doesn't say anything about it when you zero it. Thanks for any help.  

Outcomes