AnsweredAssumed Answered

How to align the timed data from transient simulation

Question asked by MSL on Jun 18, 2017

I hope to accurately compare two transient waveform by different circuit parameters, but the problem is that the time points in different simulation are not the same when I  set "timestepcontrol =trunc error".  How can resample these  waveforms into the same time axis?

Outcomes