Would like to import a vendor s-parameter dataset into the RFAMP model that Genesys already has. I have imported it into the System_Data_Folder as xxxx.sp2. I thought I read somewhere that you can use that dataset which is now in your Workspace Tree by simply cut-and-pasting the name of the dataset into the NPOD2 Model Identifier row after opening the RFAMP dialog (double-clicking on the RFAMP symbol) and opening the Manage Models dialog.
BTW, what is the difference between the NPO2 and NPOD2 entries?