Hello. I need some help about my job.
My Vee program can't recognize my equipments.
I made program on Vee9.32 for controling trque-mator Digital Torque Meter 'TS-3100A' and 'TS-3100B', Both of them are very old.
My trouble is , I can't find those meters on Vee program.
On Instrument Manager, I pushed 'Find' Button, but our trque mators haven't appeared. (other instrument appeard instantly)
I cheched up why it is, and I guess the reason below
Vee maybe use "*IDN?" to find instrumens on Instruments Manager. But my our meters support GPIB 488. Not 488.2 .
That means , they don't react the "*IDN?" and VEE Instrument Manager can't find those.
Then , does someone have idea to find those outdated Torque Meters on Vee program? I need some help.
Thanks.
First, from the VEE menu, go to File-Default Preferences-IO. Enable Pre 8.0 Legacy I/O. Next, from the instrument manager-GPIB7(Legacy)-Add a instrument. The Name could be "TS3100A". Next, in the instrument manager, select TS3100A and create a direct I/O. The direct I/O will allow commands to the TS-3100A.