AnsweredAssumed Answered

8722ES direct sampler access damage level

Question asked by alhum on May 30, 2017
Latest reply on Jul 11, 2017 by drkirkby

Hi,

 

I have a 8722ES with the direct sampler access option.

 

I would like to use a GaAs MMIC step attenuator in the sampler path. However, I have noticed that there is 0.006 V of DC offset at the step attenuator output (when measured unloaded with a multimeter). I am wondering if this present a danger to the sampler input or if I can connect this attenuator directly to the sampler input without risk.

 

Thank you for your help,

Alexis

Outcomes