AnsweredAssumed Answered

Save data from osciloscope

Question asked by surfer113 on May 25, 2017
Latest reply on May 25, 2017 by algoss

I would like to aks, if there is possiblity to save data from the osciloscope in that way, that when I use it as a logic analizer I save only time and values on the change of the bit and not values on every period that is set.

 

I need these because otherwise i cant save enough data for further analysis.

 

Im using osciloscope MSO-X 3034A

 


Thank you for your reply and help

Outcomes