I have an 8563E that recently stopped detecting signals on certain frequencies.
I have discovered that the LO signal at the front panel LO SMA connector is absent (or weaker than I am able to detect with a 437B power meter) on those frequencies where the SA does not detect signals. On those frequencies where the SA is working properly, the LO signal strength is within specs with an output of 14.58-15.95 dBm.
The error messages that I see are generally YTO-related as well: 319, 334, 356.
I suspect that this dysfunction is a result of failure of the YTO, but I am not sure where to proceed from here. I have the Service Guide 08560-90149 and I have read it but I am still not sure of my next step.
The frequencies where things are properly working include:
200 MHz
300 MHz
880-2800 MHz
5 GHz
8-12 GHz
18.9-24 GHz.
The frequencies where there is no LO signal and the SA can detect no signals are:
100 MHz
400-870 MHz
2.9-4 GHz
7 GHz
15-18.8 GHz
I would appreciate any help from the group in guiding me on how to proceed from here.
Thanks in advance and best regards,
Roger Rehr
W3SZ
If you are having signal level issues at the front panel output the problem would most likely be the A11 YTO or the A7 LO distribution amplifier. Since it appears that it is a problem in certain areas like you mention I would think that it is most likely a problem with the YTO. The problem is that you might have a problem getting a replacement since these products are beyond their support life. You could call Keysight service and see if they could still repair the instrument for you...
Mike