I don't have an answer for you, but if you like we can exchange known commands.
My current set of commands is:
FETC? → +4.718981E-08 CONF CAP CONF? → CAP +2.000000E-07,+1.000000E-11 ← this is always the range and the resolution CONF RES CONF? → RES +2.000000E+01,+1.000000E-03 CONF IMP CONF? → IMP +2.000000E+03,+1.000000E-01 CONF IND CONF? → IND +2.000000E-02,+1.000000E-06 STAT? → 0000P0P01010LL3SQ0B01 FREQ 100 FREQ 120 FREQ 1k FREQ 10k
Hi!
I don't have an answer for you, but if you like we can exchange known commands.
My current set of commands is:
FETC?
→ +4.718981E-08
CONF CAP
CONF?
→ CAP +2.000000E-07,+1.000000E-11
← this is always the range and the resolution
CONF RES
CONF?
→ RES +2.000000E+01,+1.000000E-03
CONF IMP
CONF?
→ IMP +2.000000E+03,+1.000000E-01
CONF IND
CONF?
→ IND +2.000000E-02,+1.000000E-06
STAT?
→ 0000P0P01010LL3SQ0B01
FREQ 100
FREQ 120
FREQ 1k
FREQ 10k
Bye
Hansi