AnsweredAssumed Answered

DC Bias current through N1810UL / TL RF switch max current?

Question asked by hhaisch Employee on Mar 13, 2008
Latest reply on Apr 4, 2008 by dgun
I have connected N1810UL/N1810TL RF switch to my NWA. I would like to feed a bias current via my bias-Ts in NWA via the RF switch common port to either switch port A or B. The N1810 spec indicates max. 1W Power / 7V DC voltage to termination port and 2W other. The 1W / 7V is easy to understand: 50Ohm termination resistor power handling.

However: For the through ports what is the max current the switch can handle? It would be desirable to handle up to 200-300mA?
What is the max voltage the switch can handle for the through path?  

Outcomes