AnsweredAssumed Answered

When running CAN Bus Mask testing is there any way to stop on mask violation?

Question asked by cjmontana on May 2, 2017
Latest reply on May 3, 2017 by algoss

Using MSOX3054T with the CAN Mask test. We have the digital inputs connected to circuitry before the CAN transceivers and would like to stop the testing when a mask violation occurs so we can see what the circuitry is doing on the digital inputs.

 

I have seen, on the Analyze->Setup menu an "On Error" key, but it is grayed out and not usable. I was hoping there was a way to set this to stop on error.

Outcomes