3 Weeks ago, i updated the U7243B from 3.00a to 3.20a. Also Updated Infiniium SW to 06.00.00628
(The Scope is DSO90804A with 13GHz Upgrade)
After Updated, 5G Far end Total jitter At BER-12 Test was not completed and reported following message.
Why this problem reported?
Last Version(3.00) was not reported and completed all test cases.
======================================================================================
During this run, a test reported a problem and did not complete.
If you save the project now, this information will be located in file 'IncompleteTestInfo.txt'.
Details:
Test Name: 5G Far End Total Jitter at BER-12 (CTLE ON)
Test ID: 22960
Reason: Error Performing Action on the scope
Error: Device returned SICL Error running command: :CHAN1:DISP OFF
Error: 25,"This entry isn't a valid selection. The control has not been modified."
==================================================
Details:
Keysight.DigitalTestApps.Framework.AppUtils.Sicl+SiclIOException: Device returned SICL
Error running command: :CHAN1:DISP OFF
Error: 25,"This entry isn't a valid selection. The control has not been modified."
at Keysight.DigitalTestApps.Framework.AppUtils.Sicl.CheckOutput(CheckIoArgs args)
at Keysight.DigitalTestApps.Framework.TestSteps.Steps.CommandStep.
SendCommand(Sicl io, String cmd, Boolean doSpecialPresetHandling)
==================================================
-------------------------
Recent Action History:
[3:24:22.735]CMD, :TIM:RANGE 10.0E-9
[3:24:23.240]QUERY, *IDN?
<<KEYSIGHT TECHNOLOGIES,DSO90804A,MY50140113,06.00.00628
Response Time: 0 ms
[3:24:23.338]QUERY, *OPC?
<<1
Response Time: 88.8671 ms
[3:24:23.338]QUERY, :DISP:CGRADE?
<<0
Response Time: 0 ms
[3:24:23.338]QUERY, *IDN?
<<KEYSIGHT TECHNOLOGIES,DSO90804A,MY50140113,06.00.00628
Response Time: 0 ms
[3:24:24.338]CMD, :DISPLAY:DATA? GIF, GRAT, ON, NORMAL
[3:24:26.113]QUERY, *IDN?
<<KEYSIGHT TECHNOLOGIES,DSO90804A,MY50140113,06.00.00628
Response Time: 0 ms
[3:24:26.114]CMD, :TIM:RANGE 2E-08
[3:24:26.125]CMD, :CHAN1:DISP OFF
[3:24:26.304]QUERY, :SYST:ERR? STR
<<25,"This entry isn't a valid selection. The control has not been modified."
Response Time: 178.711 ms
It appears that you may have found an 'undocumented feature', commonly called a 'bug'. You should get in touch with your local Technical Call Center and discuss this with them.
Al
Note: The Keysight Forums are designed as an informal peer-to-peer venue, and are not an appropriate way to contact Keysight Technical support.