I am looking at using a keysight 34461A bench top meter in a application where I need it to communicate to a Allen Bradley PLC ( Compact Logic 1769-L27ERM) The information I need from the meter is the resistance that the meter is reading, on a continues basis. My hope is that this has been done before and I don't have to reinvent the communications.
Hi paul002,
You can log measurements from a DMM to your PC using BenchVue and the BenchVue DMM Application.
You can either log measurements directly from the DMM Application or easily create a simple automated sequence using Test Flow
Sid