AnsweredAssumed Answered

E8362B GPIB Issues

Question asked by DavidGriff on Jan 12, 2011
Latest reply on Jan 12, 2011 by odanzy
I'm working with an E8362B Natwork Analyzer and cannot seem to get the GPIB working correctly. It is the model with only one GPIB interface. I've been able to see the instrument attached to the interface by adding the hardware using NI-488.2 hardware wizard once in system controller mode. However, once connected the device is seen all queries are getting the reply "NO MESSAGE" and the insturment information cannot be read. This happens both on Agilent IO connect wizard and MAX. I'm not sure if this is related but when using MAX it says "No Visa resources found"

I've tried reinstalling both the Agilent IO connect wizard and NI 488 but nothing has changed.  

Outcomes