AnsweredAssumed Answered

Controling external source with PNA

Question asked by Ben002 on Apr 25, 2017
Latest reply on Aug 3, 2017 by loren.betts

Hello,

I want to control an external RF source with my PNA-X. I followed all the instructions provided by the "help" section.

Hardware setup is the one following : 10 MHz out reference connected to 10 MHz in PNA

                                                             Trigger connections between PNA and external source

                                                             GB-IB interface

The PNA recognises my external source connected by GPIB (my device is available in Power Stimulus, and Frequency Stimulus). However when I want to control the source (CW or sweep frequency), nothing goes out from my source (I observe it on Spectrum analyser).

Any ideas where I got wrong?

 

Thanks

Outcomes