using matlab and or python to read an hdf5 (.h5) file that contains data from a segmented memory collect, the file has 3 groups and associated attributes, specifically the /waveform dataset has attributes of startindex, segmentedxorg and others..., i am guessing that these two are to be used to align the measurements.
1. where can i find the document which describes these variable and how they are to be used?
2. or a matlab/python would be helpful as well
thanks
You don't indicate what version of scope FW you are using, but I assume that it's recent. The format of the hdf5 files created by the scope is in the built-in help. If you have specific questions about the info in the file, that aren't answered in the help files, you can post here in the forums, or call your local Technical Contact Center. Note that the forums are not monitored on a regular basis, so calling the TCC may be better.
Al