Our analyser appears as a device in device manager on our XP machine, but when we try to launch the Agilent Logic analyser software (3.2 - this has always worked before) there is an error "Agilent Logic Analysis is either not finished or failed to initialise the system. DS1,2,3,4 are on.
When we connect to the new Win7 machine running 5.08 we do not see the device in the device manager, DS1 is off, DS2,3 are on and DS4 is on.
We've always had issues getting this machine to connect but it would be SO useful if we could get it to work now - any ideas?
It's probably a HW problem. The 1691A is, unfortunately, out of support life, and not repairable. There may be some available in the used market.
Al