This synchronous 2-wire serial link starts its frame by clocking 32 logic ones then a zero on the bi-directional data line. So a good start to decoding would be to be able to recognise this falling edge. Anyone know if the 3104 (with all decoder options enabled) can do it? Thanks
That doesn't appear to be a supported serial standard on the MSO3104, or the MSOX3000 series.