AnsweredAssumed Answered

Agilent 8164A input trigger problem

Question asked by Jason.cy001 on Mar 30, 2017
Latest reply on Mar 31, 2017 by Jason.cy001

Hi all,

    

      Any one have idea about how to externally trigger Agilent 8164A to make TLS 81640A run sweep? 

 

      I followed the user guide to set up 8164A on control panel. first, I pressed the  Config hardkey to select "Default". and Then I went to TLS channel and moved to INPUT TRIGGER MODE, Selected RUN SWEEP.  After that I used signal generator to generate a pulse signal with 2V amplitude through TRIGGER IN port. But 8164A did not make any action. Did I miss any things?

 

Thanks

 

Yue 

Outcomes