I recently purchased an HP8644B with options: 01, 05, 11. I have executed ILD diagnostics and need to execute module / cable level tests. Unfortunately, I do not posses the service kit to further diagnose the problem . Does anybody have the cable test board or schematic of the cable test board in order to build the assembly?
Hi Will02,
Normally, the schematics would be locked to the public, but since the 8644B has been obsolete for a while, we are able to share the following attachments with you (see attached schematics). It may be difficult to locate a replacement service kit, since this product is obsolete.
Note: These schematics might not be able to help if you do not know how to connect the service kit to the instrument. For help, please contact our extended service team for the 8644B:
Contact: 8644B High-Performance Signal Generator, 1 GHz or 2 GHz [Obsolete]/United States | Keysight
If you wish to speak with someone on the phone, call the toll-free number: 1 (800) 829-4444 Press #, then 2
FYI, If you are thinking about upgrading, check out this instrument:
E8663D PSG RF Analog Signal Generator, 100 kHz to 9 GHz | Keysight (formerly Agilent’s Electronic Measurement)
You may also find additional help for this product and other obsolete instruments by checking out the links on this page:
Where can I find manuals for discontinued and obsolete Hewlett-Packard, Agilent and Keysight test equipment? | Keysight
Hope this helps!
Jonathan