Dear Sir/Madam,
I am using 4395A impedance/Network analyzer to perform the impedance measurements of piezoelectric materials. I have done the calibration of both 43961A impedance test adapter and the 16093A binding post fixture. I would like to save this calibration settings in the instrument through the interface using the GPIB Commands. I tried to save the states using the command "SAVDSTA Filename" and showing the GPIB error occur on the instrument display. I can able to save states directly on the instrument using soft and hard keys and i could not able to using the GPIB command. I kindly request you to please help me in saving and recalling the calibration settings in the 4395A impedance/Network analyzer through GPIB commands.
Thanking you.
with best regards,
Sanjeev
This may be a little late as your post is from some time ago. I just viewed that post.
See images of a Keysight (Agilent) VEE Pro application I wrote quite some time ago. The images should provide an outline of the process and commands to achieve your goal.
Sincerely,
tsilchia