AnsweredAssumed Answered

Setup/Hold Time Trigger

Question asked by BOB808 on Mar 23, 2017
Latest reply on Apr 7, 2017 by algoss

I have an MSOX-4054A scope with firmware V04.08.2016071800.  For the life of me I can't get the setup/hold trigger to work.  I can set the setup time to up to <10 seconds but the max allowable hold time is stuck at <10nS.  The scope is hooked up to a relatively slow serial bus with expected setup/hold times in the uS range.  Consequently, it never triggers.

Outcomes