Hello , I need to calculate W and Wc of the offset couler by an input of Zoe Zoo s b Er
i have tried writing using SOCLIN calculator but it doest allow me this input all of them without changing the previos input parameters,
input:
Er=2.32
b=3.3
S=0.03788
output (of the book)
Wc=0.2789697
W=1.220193
the photos of the books example and the SOCLIN calculator screen are in the attached photos,
i even tried to write down the formulas in matlab ( code attached bellow) and its not giving me the result of the book.
i tried to enter the variables in the calculator in many ways
if anybody could tell me at least some way i could get this example working.
Thanks
I suggest you contact your local Technical Support department so they can thoroughly investigate. For the most accurate simulation of any transmission line structure, please consider using ADS Momentum. If you don't have the required license to run Momentum, please contact your local Keysight EEsof account representative for a demo.